VBUS.DCNOMINAL

Description

This command configures the operating DC voltage for a level other than the default of the drive.

The default nominal DC voltage is the default nominal AC voltage times square root of two.


  • The drive can be derated but do not operate it higher than the original nominal DC voltage.
  • When changed, VBUS.DCNOMINAL modifies the inrush voltage settings and the regen voltage configurations. It is important that VBUS.DCNOMINAL be set as accurately as possible to minimize voltage faults.

VBUS.DCNOMINAL and VBUS.ACNOMINAL commands are interdependent and changing the value of one will change the value of other.

VBUS.DCOPERATION determines whether AC or DC mains is being used.

Examples

If an HV drive (480Vrms) was needed for bench testing using a DC source of 170Vdc (rectified 120Vrms), do the following:

VBUS.DCOPERATION 1
VBUS.DCNOMINAL 170

General Information

Type Read/Write
Units V
Range 0 to Drive rated DC voltage
Default Value Drive’s rated DC voltage
Data Type Integer
Stored in Non-Volatile Memory Yes

Variants Supported

All variants supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

VBUS.DCNOMINAL

300ah

06h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

VBUS.DCNOMINAL

2514

9D2

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.DCNOMINAL

2514

Unsigned16

Read/Write

-

Related Topics

VBUS.ACNOMINAL

VBUS.DCOPERATION